Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 03:31 AM
This was originally posted on APC forums on 3/10/2016
I noticed that a new update was posted for the NMC2 / Symmetra 1P, so I downloaded it to see what was new (since both the old and the new versions were 6.4.0 and the release notes on the web didn't say anything).
The actual code files (aos, app, bootmon) are unchanged, although there are additional language packs included in the new build. Presumably this is to address the "***Critical: Review kbase FA280684 prior to upgrade***" issue with languages changing after 6.4.0 is installed. The KB article should probably be revised to indicate that the v3 version of the kit addresses the problem.
There is another issue with the kit - an extraneous file named "apc_hw05_aos640_sy640_bootmon108_v3" (no suffix) got included in the kit. It is actually a zip file containing aos619a, sy618b, and bootmon108. You probably want to remove this, if for no other reason that it needlessly doubles the size of the download.
Posted: 2021-06-28 03:32 AM
This reply was originally posted by Angela on APC forums on 3/14/2016
Hi John,
Thanks. Yes, I was informed of that myself when investigating the Symmetra firmware issue. We'll be fixing both file downloads shortly.
Posted: 2021-06-28 03:31 AM
This reply was originally posted by Angela on APC forums on 3/11/2016
Hi Terry,
I'll ask someone to check into it and also update the kbase.
Posted: 2021-06-28 03:31 AM
This reply was originally posted by Angela on APC forums on 3/11/2016
Hi Terry,
At this time, I think we will fix the file and also add a note in the release notes for anyone who got the version you did. Then, we will also update the download hashes/checksum.
Either way, the actual .bin files are not affected and still OK to use. Same with the language packs. But, like you said, the download size has doubled and users may be concerned that this file is needed or causes a problem when in reality it is harmless.
Thanks again for bringing it up and asking.
Posted: 2021-06-28 03:31 AM
This was originally posted on APC forums on 3/13/2016
Angela,
Looks like there is the same problem in download sumx640.
10/17/2014 03:07 PM 3,717,326 apc_hw05_aos640_sumx640_bootmon108
02/23/2016 07:11 PM 2,974,464 apc_hw05_aos_640.bin
11/05/2014 06:28 PM 262,144 apc_hw05_bootmon_108.bin
02/23/2016 07:11 PM 2,949,684 apc_hw05_sumx_640.bin
02/23/2016 07:18 PM 136 config.txt
03/13/2016 11:20 AM 0 filelist.txt
08/14/2013 11:58 AM 1,577,472 FW_Upgrade_R2.exe
08/02/2013 11:42 AM 766 FW_Upgrade_R2_se_4pp.ico
06/20/2013 11:57 AM 733 iplist.txt
02/28/2016 05:05 PM 803,103 sumx_640_esEszhCnjaJaptBrkoKo.lpk
02/28/2016 05:05 PM 816,875 sumx_640_frFrdeDeitItesEsptBr.lpk
02/28/2016 05:05 PM 926,933 sumx_640_frFrdeDeruRuitItesEs.lpk
02/28/2016 05:05 PM 920,567 sumx_640_frFrruRuzhCnjaJakoKo.lpk
03/04/2010 05:26 PM 102,912 winftp32.dll
03/04/2010 05:26 PM 89,924 winftp32.lib
Posted: 2021-06-28 03:32 AM
This reply was originally posted by Angela on APC forums on 3/14/2016
Hi John,
Thanks. Yes, I was informed of that myself when investigating the Symmetra firmware issue. We'll be fixing both file downloads shortly.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.