Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79503members
344311posts

Is there any way to stop PowerChute PE 3.0.2 alert window from appearing?

Solved
z.fake_apc
Crewman
Crewman
0 Likes
1
135

Is there any way to stop PowerChute PE 3.0.2 alert window from appearing?

This was originally posted on APC forums on 6/25/2013


Power supply to my house is really terrible, especially in evenings, as there are frequent voltage dips and peaks. While this is a problem in itself, it does not regard PowerChute. What actually does is that PowerChute's alert messagebox is highly annoying, appearing on top of most open applications and leading to unproductive clicks, especially when appearing at least once per minute. UPS' LED is already quite satisfactory as a power supply problem indicator, so is there any way to stop this super annoying window from appearing?

Method of turning off ANY of PowerChute's alert windows are even more desirable.

If of any concern, used PowerChute version is as shown in title, and my OS is Windows 7 x64.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
134

Re: Is there any way to stop PowerChute PE 3.0.2 alert window from appearing?

This reply was originally posted by Bill on APC forums on 6/26/2013


Open PowerChute and go to Options and deselect "Always show icon on the taskbar" This will stop the pop-up messages.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
135

Re: Is there any way to stop PowerChute PE 3.0.2 alert window from appearing?

This reply was originally posted by Bill on APC forums on 6/26/2013


Open PowerChute and go to Options and deselect "Always show icon on the taskbar" This will stop the pop-up messages.