Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79360members
344060posts

InRow Standalone Cooling System ACSC100 - Condensate pump cannot keep up

johnruffing_apc
Ensign
Ensign
0 Likes
0
69

InRow Standalone Cooling System ACSC100 - Condensate pump cannot keep up

This was originally posted on APC forums on 8/1/2007


Is anyone else having trouble with the ACSC100 standalone cooling unit condensate pumps not being able to keep up with removing the condensate water?

We have been having this problem for some time now and the units will SHUT DOWN. Fortunately, we have the building system HVAC as a backup in our small data center.

Since we have had this problem, even in the winter when humidity is typically low (Michigan), and we have seen this with both units, I suspect that there may be an issue with the pump itself.

Are we the only ones encountering this problem?

John