Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80572members
346459posts

FJX3000RMHV2UNC UPS: A battery bus soft start fault exists. Need some desperate help.

Solved
saeed.mulla_apc
Cadet
0 Likes
1
1387

FJX3000RMHV2UNC UPS: A battery bus soft start fault exists. Need some desperate help.

This was originally posted on APC forums on 9/4/2016


Hi APC and fellow APC UPS users.  Need some desperate help.

Just installed a standby unit (fujitsu Siemens branded APC) that was sitting around for a new environment and upon switching it on I get the following error:

"UPS: A battery bus soft start fault exists."

I have upgraded Network Monitoring 2 card to latest firmware but still getting the error.  

I have tried self test on the UPS - but says "refused" via web GUI and front panel.  If I was to remove the mains power, the UPS switches off straight away- even though the battery is showing 100% charged and 1hr+ available battery time.

The UPS comes with a 3 year warranty- but i think i may have passed that period (need to dig out receipt from emails).  

Where do I stand as its probably had less than few days of usage for something that cost me £1200+ GBP.


Accepted Solutions
voidstar_apc
Janeway
Janeway
0 Likes
0
1387

Re: FJX3000RMHV2UNC UPS: A battery bus soft start fault exists. Need some desperate help.

This was originally posted on APC forums on 9/5/2016


If those batteries are three years old, then they're dead. Anything over 6 months is pushing it.

See Answer In Context

1 Reply 1
voidstar_apc
Janeway
Janeway
0 Likes
0
1388

Re: FJX3000RMHV2UNC UPS: A battery bus soft start fault exists. Need some desperate help.

This was originally posted on APC forums on 9/5/2016


If those batteries are three years old, then they're dead. Anything over 6 months is pushing it.