Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79539members
344371posts

Energy Usage not visible and Energy Management not working

Solved
carreiror_apc
Cadet
0 Likes
2
216

Energy Usage not visible and Energy Management not working

This was originally posted on APC forums on 5/21/2011


Hi,


I just bought an UPS backup model BE700G-SP (written in unit), and I was looking for the Energy Usage page (under the Monitor System tab), but it's not visible, should it be there?

Also when I activate the Energy management, under Configuration tab, it automatically turns off the outlets, and the “Turn Power On” button does not work!
It this unit, OK?

I'm using PowerChute Personal Edition 3.0

I bought this model for the ability to monitor Power usage, if this does not work I would have bought from another vendor a 30 Eur unit... and would not spend 100eur!!!!!

PS: Windows 7 Ultimate 64bits ; i3 530 ; P


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
217

Re: Energy Usage not visible and Energy Management not working

This reply was originally posted by Bill on APC forums on 2/23/2015


David,

The BE550G does not offer those features. If you would like those features with a BE style unit you should purchase a BE750G.

See Answer In Context

2 Replies 2
deardavid_apc
Crewman
Crewman
0 Likes
0
217

Re: Energy Usage not visible and Energy Management not working

This was originally posted on APC forums on 2/21/2015


I just got PowerChute v3.0.2 for my BE550G, and it has no Energy Usage or Run Self-Test tabs under Monitor System

BillP
Administrator Administrator
Administrator
0 Likes
0
218

Re: Energy Usage not visible and Energy Management not working

This reply was originally posted by Bill on APC forums on 2/23/2015


David,

The BE550G does not offer those features. If you would like those features with a BE style unit you should purchase a BE750G.