Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80775members
346794posts

Do these units need batteries to power on?

Solved
computronium_apc
Cadet
0 Likes
2
69

Do these units need batteries to power on?

This was originally posted on APC forums on 4/27/2016


I have received a few UPSs and I plugged them in but they didn't seem to power on. My question is this, do they need batteries in them to even power on? I plugged them in and there was no response to button presses or anything. The models that I have are SmartUPS 700 and SmartUPS1000. I think they are older ones and they are white, not the black newer ones. Thank you for your time.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
69

Re: Do these units need batteries to power on?

This reply was originally posted by Gareth on APC forums on 4/27/2016


SMT does not, I can at least confirm that!

See Answer In Context

2 Replies 2
voidstar_apc
Janeway
Janeway
0 Likes
0
71

Re: Do these units need batteries to power on?

This was originally posted on APC forums on 4/27/2016


Depends on the exact model. If the model starts with SUA, then it needs a good battery. SMX, SMT, and I think SMC do not.

BillP
Administrator Administrator
Administrator
0 Likes
0
70

Re: Do these units need batteries to power on?

This reply was originally posted by Gareth on APC forums on 4/27/2016


SMT does not, I can at least confirm that!