Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80901members
347020posts

Connecting Devices to Smart UPS

Solved
goodfella_apc
Ensign
Ensign
0 Likes
4
202

Connecting Devices to Smart UPS

This was originally posted on APC forums on 2/16/2016


Hi,

       I have APC Smart UPS SUA1500i model line interactive UPS (1500 VA). My doubt is whether I can

cannect my HP SCANJET 2400 Flatbed scanner directly to the UPS using the power cord supplied by HP,

in addition to my DESKTOP and LCD Monitor. Also since there are additional power slots in the UPS can I

connect a Printer (Except Laser Printer) directly to the UPS. Please help. Thanks in advance.

Regards,

Jayan.


Accepted Solutions
goodfella_apc
Ensign
Ensign
0 Likes
0
202

Re: Connecting Devices to Smart UPS

This was originally posted on APC forums on 2/17/2016


Thank you Bill and Joe. Got it.

See Answer In Context

4 Replies 4
BillP
Administrator Administrator
Administrator
0 Likes
0
202

Re: Connecting Devices to Smart UPS

This reply was originally posted by Joe on APC forums on 2/16/2016


You can connect as many devices to the UPS as you can as long as you do not overload the UPS.  Laser printers, as you've noted, uses quite a bit of power when the fuser is in operation and this is why connecting a laser printer to a UPS is keeping with good practices.

The HP Scanjet 2400 is acceptable load and will do fine on your Smart UPS.

goodfella_apc
Ensign
Ensign
0 Likes
0
202

Re: Connecting Devices to Smart UPS

This was originally posted on APC forums on 2/16/2016


Hi Joe,

           Thank you. For the explanation. Actually my doubt is regarding the power cord supplied by HP along with the 

SCANJET. Also there are power cables coming with printers. Can I plug in those cables to the rear slots in the APC

UPS ? There are 4 or 6 sockets at the back of the APC UPS. Like plugging in to the main utility, can I plug into the

UPS directly? Please reply.

Thanks & Regards,

Jayan.

BillP
Administrator Administrator
Administrator
0 Likes
0
202

Re: Connecting Devices to Smart UPS

This reply was originally posted by Bill on APC forums on 2/16/2016


Hi,

Yes you can plug the scanjet directly into the UPS as long as you do not overloaded the UPS as mentioned by Joe. 

goodfella_apc
Ensign
Ensign
0 Likes
0
203

Re: Connecting Devices to Smart UPS

This was originally posted on APC forums on 2/17/2016


Thank you Bill and Joe. Got it.