Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 10:46 PM
This was originally posted on APC forums on 2/16/2016
Hi,
I have APC Smart UPS SUA1500i model line interactive UPS (1500 VA). My doubt is whether I can
cannect my HP SCANJET 2400 Flatbed scanner directly to the UPS using the power cord supplied by HP,
in addition to my DESKTOP and LCD Monitor. Also since there are additional power slots in the UPS can I
connect a Printer (Except Laser Printer) directly to the UPS. Please help. Thanks in advance.
Regards,
Jayan.
Posted: 2021-06-30 10:46 PM
This was originally posted on APC forums on 2/17/2016
Thank you Bill and Joe. Got it.
Posted: 2021-06-30 10:46 PM
This reply was originally posted by Joe on APC forums on 2/16/2016
You can connect as many devices to the UPS as you can as long as you do not overload the UPS. Laser printers, as you've noted, uses quite a bit of power when the fuser is in operation and this is why connecting a laser printer to a UPS is keeping with good practices.
The HP Scanjet 2400 is acceptable load and will do fine on your Smart UPS.
Posted: 2021-06-30 10:46 PM
This was originally posted on APC forums on 2/16/2016
Hi Joe,
Thank you. For the explanation. Actually my doubt is regarding the power cord supplied by HP along with the
SCANJET. Also there are power cables coming with printers. Can I plug in those cables to the rear slots in the APC
UPS ? There are 4 or 6 sockets at the back of the APC UPS. Like plugging in to the main utility, can I plug into the
UPS directly? Please reply.
Thanks & Regards,
Jayan.
Posted: 2021-06-30 10:46 PM
This reply was originally posted by Bill on APC forums on 2/16/2016
Hi,
Yes you can plug the scanjet directly into the UPS as long as you do not overloaded the UPS as mentioned by Joe.
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.