Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79239members
343869posts

Clear lost communications

Solved
tlilkov_apc
Crewman
Crewman
0 Likes
2
177

Clear lost communications

This was originally posted on APC forums on 11/2/2015


Hello,

I am using Smart-UPS RT 6000 XL I have removed the temperature sensor. Now I have alarm "lost communication" which I want to clear (of course without any effect of UPS outputs) for this I need of your help!

Thank you in advance!!!

PrtScn

Attachments

Accepted Solutions
tlilkov_apc
Crewman
Crewman
0 Likes
0
177

Re: Clear lost communications

This was originally posted on APC forums on 11/2/2015


I made restart on the management card and now all it is fine.
Thanks.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
177

Re: Clear lost communications

This reply was originally posted by Angela on APC forums on 11/2/2015


You can warm reboot the network management card interface (which does not affect the UPS output power). Go to Control->Network->reset/reboot and select restart management interface and then apply and carry out that action and the alarm should clear. There is an option in there to Reset Only: "Lost Environmental Communication Alarms" but I think there was a bug with it not working in certain firmware versions. You can try that first if you want if not, restart the management interface to clear it for sure.

tlilkov_apc
Crewman
Crewman
0 Likes
0
178

Re: Clear lost communications

This was originally posted on APC forums on 11/2/2015


I made restart on the management card and now all it is fine.
Thanks.