Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80810members
346870posts

CAP - Cybersecurity Application Platform, connection error in the web interface

MarcoAntonio_C
Cadet
Cadet

CAP - Cybersecurity Application Platform, connection error in the web interface

I installed the CAP in a Linux VM but when I try to open the OT dashboard to view the Graylog in the Google Chrome(in the same PC but in the windows) it shows the error 502 Bad Gateway.

 

I don't know if I skipped a step in the installation process or there are some connection problems due to the fact that I created a loopback adapter to connect the VM to the main OS.

 

When I run the command to view the process that are running in the Linux it appears that the Graylog is off. Is there some way that I can manually start it? 

 

Thanks in advance  

Tags (1)