Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79399members
344145posts

Battery Power Alert

andre.claudino_apc
Crewman
Crewman
0 Likes
0
123

Battery Power Alert

This was originally posted on APC forums on 6/17/2016


Hello Dear,


I have received a message alert from UPS:

UPS: A discharged battery condition no longer exists.    0x0108
UPS: The battery power is too low to support the load; if power fails, the UPS will be shut down immediately.    0x0107


But the battery is full, as can see in the picture "Print 1.

I checked physically the UPS and it's OK. Both the Battery Leds and Load Leds are Ok.


Thank You In advanded!

Tags (1)