Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 06:22 AM
This was originally posted on APC forums on 2/9/2012
Hello all,
I am programming a little bash script that checks whether a machine is down or not, and if yes, it reboots the machine.
For doing so, it needs to connect to the PDU and launch the "reboot" command on the outlet to which the machine is connected.
The problem is that I want this to be automated but the ssh (and telnet) connection keeps asking me for the password... Isn't it possible to install a key certificate so that password is not required during my script execution?
I've read the manual but I can't figure out how to run automated scripts on the PDU.
Any ideas on this?
Thanks in advanced!!
Pedro
Posted: 2021-06-28 06:22 AM
This was originally posted on APC forums on 2/13/2012
Hi,
After some trial and error, and a few coffees too, I've managed to program a simple script that does what I mentioned.
Unfortunately, a UNIX tool called "expect" is needed, which is not installed by default in all UNIX-based distribution. You can install it via apt-get or yum (depending on your distribution)
The script basically waits until a string similar to the pattern given to "expect" is written on the console prompt, and then it sends the passwords (or commands) as if they were written by the user. The script works both for telnet and ssh2 connections (can't guarantee ssh1 since my workstation hasn't got it installed).
The code is the following:
// USE ---> /ssh_command.sh user password ip
// set Variables
set user [lrange $argv 0 0]
set password [lrange $argv 1 1]
set ipaddr [lrange $argv 2 2]
set timeout -1
// now connect to remote PDU
// using TELNET---> spawn telnet $ipaddr
spawn ssh $user@$ipaddr
match_max 100000
// Using TELNET
//expect "User Name :"
//send "$user"
// Look for passwod prompt
expect "*?assword*"
// Send password aka $password
send "$password"
expect "APC>"
send "off 1"
expect "APC>"
sleep 3
send "on 1"
expect "APC>"
send "exit"
expect eof
close $spawn_id
I hope this helps anyone with the same problem.
PS:
I tried to change the fingerprint of the PDU, but that didn't work because the fingerprint identifies the PDU so when other clients connect to it, they can trust this host (the PDU). However, the PDU wasn't able to recognize clients.
Tried also to upload the fingerprint of my workstation to a directory in the PDU (specifically "~/.ssh" as it says this tutorial), but the ftp server that runs on the PDU isn't very flexible, and doesn't allow you to create folders or so.
Message was edited by: pedriyoo
Message was edited by: pedriyoo
Posted: 2021-06-28 06:22 AM
This reply was originally posted by Angela on APC forums on 2/9/2012
what model PDU is it? There is a scriping CLI on our two generations of PDUs outlined here: http://nam-en.apc.com/app/answers/detail/a_id/10853
Posted: 2021-06-28 06:22 AM
This was originally posted on APC forums on 2/9/2012
It is a AP7920 device.
I can connect to the command line, but I'd like to connect to it using a certificate, so I can make an ssh connection in a script automatically, without giving out the password.
Posted: 2021-06-28 06:22 AM
This reply was originally posted by Angela on APC forums on 2/9/2012
what SSH client are you using? i would think you could put the key in its keystore but i guess i have never tried. i am not sure if there is a way to get around typing the password completely 😕
Posted: 2021-06-28 06:22 AM
This was originally posted on APC forums on 2/13/2012
Hi,
After some trial and error, and a few coffees too, I've managed to program a simple script that does what I mentioned.
Unfortunately, a UNIX tool called "expect" is needed, which is not installed by default in all UNIX-based distribution. You can install it via apt-get or yum (depending on your distribution)
The script basically waits until a string similar to the pattern given to "expect" is written on the console prompt, and then it sends the passwords (or commands) as if they were written by the user. The script works both for telnet and ssh2 connections (can't guarantee ssh1 since my workstation hasn't got it installed).
The code is the following:
// USE ---> /ssh_command.sh user password ip
// set Variables
set user [lrange $argv 0 0]
set password [lrange $argv 1 1]
set ipaddr [lrange $argv 2 2]
set timeout -1
// now connect to remote PDU
// using TELNET---> spawn telnet $ipaddr
spawn ssh $user@$ipaddr
match_max 100000
// Using TELNET
//expect "User Name :"
//send "$user"
// Look for passwod prompt
expect "*?assword*"
// Send password aka $password
send "$password"
expect "APC>"
send "off 1"
expect "APC>"
sleep 3
send "on 1"
expect "APC>"
send "exit"
expect eof
close $spawn_id
I hope this helps anyone with the same problem.
PS:
I tried to change the fingerprint of the PDU, but that didn't work because the fingerprint identifies the PDU so when other clients connect to it, they can trust this host (the PDU). However, the PDU wasn't able to recognize clients.
Tried also to upload the fingerprint of my workstation to a directory in the PDU (specifically "~/.ssh" as it says this tutorial), but the ftp server that runs on the PDU isn't very flexible, and doesn't allow you to create folders or so.
Message was edited by: pedriyoo
Message was edited by: pedriyoo
Posted: 4 weeks ago
Hello,
Thanks for your provided the script, I have tried and found when I running the script ssh to PDU, but hung when I running the script.
# ./apc.sh apc apc 192.168.1.7
spawn ssh apc@192.168.1.7
apc@192.168.1.7's password: apc
Do you know the reason?
Thank you.
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.