Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80657members
346640posts

Accessing Network Management Card #AP9619

Solved
electriceye_apc
Ensign
Ensign
0 Likes
5
215

Accessing Network Management Card #AP9619

This was originally posted on APC forums on 2/21/2011


Hello All-

We have a Network Management Card #AP9619 in our SymmetraF UPS. Card has activity lights and such but we cannot seem to access it over our LAN. Is there a way to reset the card to DHCP? I did see a little reset pin area on the back plate of the card but am not convinced it actually reset. The way I see it, if it reset to defaults it should puick up an IP address right away. I scoped my LAN with Orion Lan Surveyor, however and could not see it anywhere. FYI- I already found this KB article and seem to be at an impasse.

http://emea-en.apc.com/app/answers/detail/a_id/3061/~/how-do-you-make-a-network-management-card-comm...


Accepted Solutions
seoerming1_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
215

Griffey Shoes

This was originally posted on APC forums on 3/23/2011


"That just tells you Syracuse wasn't that Griffey Shoes good," Barkley retorted. There will probably be people Air Jordan Heels who agree with Barkley that only eight Big East teams belonged in the NCAA tournament Ken Griffey Shoes as a result of the conference's awful showing, but the truth is the league simply performed well below Air Max 24 7 expectations in single-elimination format. Based on their season-long body of work, it would have been very difficult to justify leaving Nike Air Yeezy out Connecticut, Villanova or Marquette, the teams that finished ninth, 10th and 11th in the Big East regular-season standings. Even Nike Dunk Heels though he had the more logical argument, Pitino didn't exactly help himself when he looked straight into the camera and guaranteed "Notre Dame will not lose" Sunday night against Florida State. The lesson here: Never pin your TV credibility to Notre Dame in the NCAA tournament and never argue with Barkley even when you're right.

See Answer In Context

5 Replies 5
upsguy_apc
Commander
Commander
0 Likes
0
216

Re: Accessing Network Management Card #AP9619

This was originally posted on APC forums on 2/21/2011


If the reset function isn't working the card probably has had a Static IP configured. I'm not sure what type a SymmetraF UPS is but the larger Symmetra systems allow you to serial into the NMC via the serial port using the 0024C or D cable. Do you have this cable? DO NOT TRY TO SERIAL IN WITH ANYTHING OTHER THAN THIS CABLE, YOU RISK A LOAD LOSS WITH A NORMAL SERIAL CABLE.

electriceye_apc
Ensign
Ensign
0 Likes
0
216

Re: Accessing Network Management Card #AP9619

This was originally posted on APC forums on 2/21/2011


upsguy-

Thanks for the reply- unfortunately we do not have the desigamated serial cable. And yes, I had heard stories of that problem before so I resisted the temptation of digging out a standard RS-232 cable. I thought that maybe you could shunt a pin or two together to reset it while under power than power down and remove the card and remove the shunt. I will pull the card again and look at the reset recess, maybe we didn't hit it correctly.

Thanks again!

electriceye_apc
Ensign
Ensign
0 Likes
0
216

Re: Accessing Network Management Card #AP9619

This was originally posted on APC forums on 2/22/2011


upsguy-

I just had a hair-brained idea...maybe connect the NM card to a small switch or better yet hook up a LAN crossover cable and check it with a laptop. Maybe a netstat or other command might show me what the IP of the card is. I suppose I could even use my laptop (with LAN surveyor on it) this way and let it discover what the IP of the card is... just a thought...

Elec_apc
Ensign
Ensign
0 Likes
0
216

Re: Accessing Network Management Card #AP9619

This was originally posted on APC forums on 2/22/2011


Try to configure you nmc with the apc software ( APC device ip configuration wizard) linked with network cable to your nmc, and don't forget to configure the lan port of pc with the same range of ip address.
example if you need to configure the nmc with tcp/ip:192.168.1.4, the configuration tcp/ip of your pc port must be :192.168.1.10
if you want to make your own serial cable to communicate with the nmc through serial com,i can give you the pin configuration upon request.
NOTE: the reset button is not useful without the serial com and hyper terminal program.

Message was edited by: Elec

seoerming1_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
216

Griffey Shoes

This was originally posted on APC forums on 3/23/2011


"That just tells you Syracuse wasn't that Griffey Shoes good," Barkley retorted. There will probably be people Air Jordan Heels who agree with Barkley that only eight Big East teams belonged in the NCAA tournament Ken Griffey Shoes as a result of the conference's awful showing, but the truth is the league simply performed well below Air Max 24 7 expectations in single-elimination format. Based on their season-long body of work, it would have been very difficult to justify leaving Nike Air Yeezy out Connecticut, Villanova or Marquette, the teams that finished ninth, 10th and 11th in the Big East regular-season standings. Even Nike Dunk Heels though he had the more logical argument, Pitino didn't exactly help himself when he looked straight into the camera and guaranteed "Notre Dame will not lose" Sunday night against Florida State. The lesson here: Never pin your TV credibility to Notre Dame in the NCAA tournament and never argue with Barkley even when you're right.