Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-01 01:55 AM
This was originally posted on APC forums on 12/3/2012
Hi I have a APC Symmetra 12Kva what software can i use to read alarm´s Amp´s volt... so on..
Thank´s
Message was edited by: rebotea
Posted: 2021-07-01 01:55 AM
Posted: 2021-07-01 01:55 AM
This reply was originally posted by Angela on APC forums on 12/4/2012
any symmetra comes with a pre-installed network management card that provides this information. you can assign a network address to it and access it via IP. can you check the rear of the symmetra to see if you see an RJ-45 network jack with a model of card such as AP9606, AP9619 or AP9631?
Posted: 2021-07-01 01:55 AM
This was originally posted on APC forums on 12/4/2012
Yes it has. mainly i only have to conect to the card no need for software right!!!!!!!!.
Posted: 2021-07-01 01:55 AM
This reply was originally posted by Angela on APC forums on 12/4/2012
yes, that is correct. you would only then use powerchute network shutdown when you are trying to gracefully shutdown clients attached to the UPS. the network management card in the UPS provides the data you mentioned though.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.