Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 07:50 AM
This was originally posted on APC forums on 3/14/2014
Hi there,
I have an APC UPS SUA1500i, bought it approximately three years ago.
At the very beginning when I started connecting the cables to connect all the equipment I noticed that the rear output connectors/receptacles(?) -- there are 8 of them -- are slightly moving. Tried using the cables supplied with the UPS and also bought some more, and noticed that at the slightest pull or touch they just simply move, causing electricity fall-outs, and could even fall out. And sometimes, when vacuum-cleaning around the UPS and its cables, should I touch any of the output cables, electricity to device(s) falls-out, sometimes there’s even that electrical ‘buzzing’ sound.
What use is the UPS when it has electricity but the output cables are moving and do not provide proper electrical supply? Three SATA disks were destroyed in the recent power fall-out.
Also, what is the meaning of all the LED lights on the right blinking very fast? If I work with the laptop, they aren't lit, but if I turn on the desktop computer, they start blinking.
Anyone else had this issue? Help me, please.
Posted: 2021-06-29 07:50 AM
This was originally posted on APC forums on 3/24/2014
An update to my issue with loose cables...
What I did to fix this is with plastic furniture levelers. Strange, but it works! Cables don't move any longer.
Posted: 2021-06-29 07:50 AM
This reply was originally posted by Angela on APC forums on 3/17/2014
I can tell you about the flashing battery bar graph here...
Why are the battery charge LEDs flashing on a Smart-UPS? | FAQs | Schneider Electric ITB
Usually this means that there is a setting/configuration issue or that the runtime is low if you haven't changed any settings recently.
Posted: 2021-06-29 07:50 AM
This was originally posted on APC forums on 3/24/2014
Thank you for your answer, Angela. Have to read the document and try what can be done.
Posted: 2022-04-07 12:15 AM
Hi Could you please post a link to the plastic furniture levelers?
User | Count |
---|---|
4836 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.