Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 09:47 PM
This was originally posted on APC forums on 4/20/2009
Will APC ever produce new firmware for the AP9617 that supports SMTP Authentication? I purchased a SmartUPS and network management card with the intent of utilitzing the email alert feature to notify me of a power outage. However I quickly learned that the card does not support authentication. To me this is a serious limitation of APC's product since most SMTP servers require authentication.
Posted: 2021-06-28 09:47 PM
This reply was originally posted by Angela on APC forums on 9/2/2009
yes. it will be in version 5.1.0 for AP9630, AP9631, and AP9635 only, ETA is Q1 2010 for this release - most likely early Q1..
also in 5.1.0 will be IPv6, localized language packs, and Modbus Over TCP to name a few features.
Posted: 2021-06-28 09:47 PM
This was originally posted on APC forums on 4/20/2009
Hello there,
Well I have some good news and not so good:
- SMTP authentication is on the roadmap for development - a very rough timeline is Q1 2010 (please don't hold me to that!)
The firmware that will feature this support will be for the new generation of network cards that were just released: AP9630, AP9631. These two sku's are the respective replacements for the AP9617 and AP9619. In APC's commitment to provide the latest and greatest firmware features, it was necessary to shift to a more robust piece of hardware to drive the code. The new cards allow some breathing room to run the code that will eventually boast new features (IPv6, more robust security algorithms, etc) as well as some hardware considerations for additional features (such as USB port).
I hope this helps! I'll keep an eye on this thread should you need any further support.
Posted: 2021-06-28 09:47 PM
This reply was originally posted by Angela on APC forums on 9/2/2009
yes. it will be in version 5.1.0 for AP9630, AP9631, and AP9635 only, ETA is Q1 2010 for this release - most likely early Q1..
also in 5.1.0 will be IPv6, localized language packs, and Modbus Over TCP to name a few features.
Posted: 2021-06-28 09:47 PM
This was originally posted on APC forums on 9/1/2009
Hi, any update on the timeline for the new AP9630 firmware that will handle email authentication?
User | Count |
---|---|
4836 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.