Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-09 04:02 AM
This question was originally posted by Hosein on APC forums on 11/7/2015
hello
i have Installed an APC AP8853 recently . the PDU works and output works correctly but I can't see any things on the PDU LCD !! all LCD display is just green !
how can i fix it ?
PDU serial n. 5A1436e04877
thanks
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Angela on APC forums on 1/25/2016
Hi again,
You have to contact your local support office via http://www.apc.com/site/support/index.cfm/contact-information/ for further help. We can't provide RMA or warranty support via the forum.
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Tom on APC forums on 11/9/2015
Hosein,
Sorry to hear that your having some trouble.
Check out this out this knowledge base:
If this doesn't work you may need to call into tech support. The unit does appeared to still be under warranty.
Tom
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Angela on APC forums on 11/9/2015
A blank display can also indicate a generic firmware problem. The PDU has an AOS (APC Operating System) and application file. If the application file populates and runs the display. If the file is not there or is the incorrect one, the LCD will not work.
I recommend you check the knowledge base above but also clarify what LEDs are present on the LCD screen and what color/pattern they are, as well as if you're able to serial in to the device using the included 940-0144 serial communication cable @ 9600 baud rate.
From there, you'd be able to see what is going on with the firmware. If you just installed it and powered it up, I would doubt it is the article Tom noted above but it could be..
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Hosein on APC forums on 12/22/2015
Dear Angela
i read the knowledge base and checked the above link . i can't access to PDU with my PC so i can't update The PDU . the pdu accept no IP .i can't set any IP to PDU .
i took a picture of PDU and attached below .
what's your idea about replacing the AP9537 board on PDU ?
for more info , the pdu PDU has output power.
thank you very much .
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Angela on APC forums on 12/22/2015
Did you attempt to access the PDU via a serial connection/bootmonitor mode as per the knowledge base (since you can't set an IP or access it normally)?
This is a metered rack PDU so even if there is a problem with the display/management interface, the outlets will still provide power. This is not necessarily the case on a switched rack PDU.
If you cannot access the device via serial connection/bootmonitor as outlined in the knowledge base article, then your local technical support team can provide a replacement display, assuming the Rack PDU is under warranty. Otherwise, they may be able to sell you the display as a spare part.
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Hosein on APC forums on 1/25/2016
Posted: 2021-07-09 04:03 AM
This reply was originally posted by Angela on APC forums on 1/25/2016
Hi again,
You have to contact your local support office via http://www.apc.com/site/support/index.cfm/contact-information/ for further help. We can't provide RMA or warranty support via the forum.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.