Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80874members
346978posts

ACRC100 Unit Configuration

torchedya_apc
Cadet

ACRC100 Unit Configuration

I am configuring an ACRC100 cooling unit. Under the unit tab on the web interface it is asking for power source. The options are Source A, Source B, Source A and B. Can anyone tell me what this does? What happens if I have two sources but only choose one?

Tags (1)