Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80976members
347151posts

3000XL Fan Always on

Solved
jimm_apc
Cadet
0 Likes
4
132

3000XL Fan Always on

This was originally posted on APC forums on 2/16/2014


Hi,
I have a 3000XL UPS. It used to live in a comms cupboard but due to an office move I now need it to live in the same room as staff.

Upon moving the UPS to its new location I have found the fan seems to run constantly. Im not sure if it did this in the old location.

Is this normal?

Is there a way to stop it?

Its not hot (internal temp is 22^C), no errors in the logs.

It is only running slow (not the fast like when its on battery or charging) but it is noisy enough to annoy staff.

So can anyone say is this is typical?

Thanks

Tags (1)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
132

Re: 3000XL Fan Always on

This reply was originally posted by Angela on APC forums on 2/18/2014


Yes, SUA3000XLI has a fan that is always on with high/low fan speeds. How old is it? If you have the first 6 digits of the UPS serial number I can tell you. It could either be very dirty and dusty and use some cleaning or if that's not the case, it could have a noisy bearing perhaps. A UPS does have a hum, especially when operating on battery, but it shouldn't be so noisy and distracting..

See Answer In Context

4 Replies 4
BillP
Administrator Administrator
Administrator
0 Likes
0
132

Re: 3000XL Fan Always on

This reply was originally posted by Angela on APC forums on 2/17/2014


Can you confirm the exact SKU of the UPS? This is on the white sticker on the back of the UPS.

I ask because some newer models have a low/high fan mode in order to keep the UPS as cool as possible. Other models just use the fan typically if the UPS internal temperature is too warm, if the UPS has a high load over 75%, if the UPS is on battery, or if the UPS is charging the battery.

Once I know the model of UPS, I can verify the behavior of the particular model. If it is one with the low/high mode, then is it possible the fan is dirty? If that is the case, then I'd suggest maybe try cleaning it with compressed air. Usually a Smart UPS is installed in a data center or server room so I don't think noise is typically a primary concern but even so, I have not encountered one that I would say on low is too noisy to annoy everyone even outside of a server room environment.

jimm_apc
Cadet
0 Likes
0
132

Re: 3000XL Fan Always on

This was originally posted on APC forums on 2/17/2014


Hi,

The full model code is "SUA3000XL I"

There is currently no load on it, its not on battery and shouldnt be charging (reports 100% battery and been on mains for the weekend).

Thanks

Battman_apc
Commander
Commander
0 Likes
0
132

Re: 3000XL Fan Always on

This was originally posted on APC forums on 2/17/2014


FYI if this Tower SUA3000 is similar inside to the SUA3000 rack mount versions I look after hundreds of there could be upwards of three fans inside, but more likely two. In the rack mount a large one cools the main inverter, a smaller one is immediately beside that one for side by side flow to cool the transformer pair/mainboard, and a third (smallest one) is cooling the batteries. All three fans run continuously in the rack mount version...

BillP
Administrator Administrator
Administrator
0 Likes
0
133

Re: 3000XL Fan Always on

This reply was originally posted by Angela on APC forums on 2/18/2014


Yes, SUA3000XLI has a fan that is always on with high/low fan speeds. How old is it? If you have the first 6 digits of the UPS serial number I can tell you. It could either be very dirty and dusty and use some cleaning or if that's not the case, it could have a noisy bearing perhaps. A UPS does have a hum, especially when operating on battery, but it shouldn't be so noisy and distracting..