Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 11:15 PM
This was originally posted on APC forums on 11/22/2009
it is hot, as in i can't hold my hand against it for longer than a few seconds.... wanting to make sure this is normal. batteries indicate fully charged, and disconnecting from shore power results in failover to battery (so the thing appears operational).
thanks
Posted: 2021-06-28 11:15 PM
This reply was originally posted by Jonathan on APC forums on 11/23/2009
Jim,
What is the model and serial number of the UPS? The batteries that are on the UPS, are they the original ones that came with the unit? When did this problem started? Also, would it be possible for you to open the battery compartment to check its condition, check for signs of swelling, bulging, venting or leaks. Also, see if you can still remove the batteries from the unit itself.
JonPro
Posted: 2021-06-28 11:15 PM
This reply was originally posted by Vkooldog on APC forums on 11/23/2009
Hi,
If your batteries are too hot to touch, it means that the deployment conditions of that unit may not be suitable. A raise in temperature will shorten the lifespan of the UPS ( compoments ) and the batteries life.
What I would suggest is to move the unit to a more cooler environment and monitor its internal temperature thru APC software and take steps to keep the environment temperature of the UPS to its operating environment eg below 25 degress Celcius.
Regards
Message was edited by: kooldog007
Message was edited by: kooldog007
Posted: 2021-06-28 11:15 PM
This reply was originally posted by Vkooldog on APC forums on 11/23/2009
If your batteries are too hot to touch, it means that the deployment conditions of that unit may not be suitable. A raise in temperature will shorten the lifespan of the UPS ( compoments ) and the batteries life.
What I would suggest is to move the unit to a more cooler environment and monitor its internal temperature thru APC software and take steps to keep the environment temperature of the UPS to its operating environment eg below 25 degress Celcius.
Regards
Posted: 2021-06-28 11:15 PM
This reply was originally posted by Jonathan on APC forums on 11/23/2009
Jim,
What is the model and serial number of the UPS? The batteries that are on the UPS, are they the original ones that came with the unit? When did this problem started? Also, would it be possible for you to open the battery compartment to check its condition, check for signs of swelling, bulging, venting or leaks. Also, see if you can still remove the batteries from the unit itself.
JonPro
User | Count |
---|---|
4836 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.