Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80846members
346932posts

Maximum Current Input for 555

Solved
BillP
Administrator Administrator
Administrator
0 Likes
2
91

Maximum Current Input for 555

This question was originally posted by miya on APC forums on 7/28/2017


I was looking over a datasheet for the NE555 Timer  and I was wondering if the max supply current given under the electrical characteristics page is the max current you can supply to the 555 without damaging the chip.

Here is the datesheet of ne555n

I ask because it seems like the supply current (for 15V input) is relatively low (10mA) compared to the output current (225mA).

Is the supply current the max current you can put on pin 8 without burning out the chip? If so, why is it so low compared to the output current? If not, how does one find the input current?


Accepted Solutions
becksamenterprises_apc
Lieutenant
Lieutenant
0 Likes
0
91

Re: Maximum Current Input for 555

This was originally posted on APC forums on 7/29/2017


I've never seen that either. Nice observation

See Answer In Context

2 Replies 2
Brad_C_apc
Commander
Commander
0 Likes
0
91

Re: Maximum Current Input for 555

This was originally posted on APC forums on 7/28/2017


The max supply current you refer to is the maximum the chip will draw (you don't supply current to a chip, you supply it a voltage and it takes what it needs) with an unloaded output. The bits you need to watch out for are the "absolute maximum rating" and there you'll want to watch the maximum power dissipation when you load the output significantly.

having said that, you are absolutely in the wrong place to ask these questions as I've never seen a 555 inside an APC product. Try the eevblog forum for electronics.

becksamenterprises_apc
Lieutenant
Lieutenant
0 Likes
0
92

Re: Maximum Current Input for 555

This was originally posted on APC forums on 7/29/2017


I've never seen that either. Nice observation