Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80627members
346583posts

Broke UPS MGE NOVA 1100 AVR and now for the repairs necessary to identify the burnt part.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
140

Broke UPS MGE NOVA 1100 AVR and now for the repairs necessary to identify the burnt part.

This question was originally posted by Oleg on APC forums on 10/15/2016


Hello! Broke UPS MGE NOVA 1100 AVR and now for the repairs necessary to identify the burnt part. Visually similar to the burned part SMD-transistor. Next to this part on the board there is an inscription "VT15". On the part itself is written as follows: (ON) RJU / AH (in fact, instead of parentheses the word "ON" is taken in a circle, and the sign "/" is used as a line separator, as the inscription consists of two lines). On the board itself has the following label: PNSBP00011BC NT02.

PS: sorry my bad english.

Tags (4)

Accepted Solutions
voidstar_apc
Janeway
Janeway
0 Likes
0
140

Re: Broke UPS MGE NOVA 1100 AVR and now for the repairs necessary to identify the burnt part.

This was originally posted on APC forums on 10/16/2016


Judging from the marking on the part, maybe On Semiconductor's BCP53?

See Answer In Context

1 Reply 1
voidstar_apc
Janeway
Janeway
0 Likes
0
141

Re: Broke UPS MGE NOVA 1100 AVR and now for the repairs necessary to identify the burnt part.

This was originally posted on APC forums on 10/16/2016


Judging from the marking on the part, maybe On Semiconductor's BCP53?