Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2022-04-28 10:00 AM
I have an APC AP 8659 PDU with an apparently corrupted rpdug2 application on it (the app status is A-). The bootmon and AOS look to be good based on the status when I ssh into the unit. The Firmware version appears to be at 6.8.0 (AOS 6.8.2, Bootmon 1.0.9), so I went to the website to try to download 6.8.0, but every 6.8.0 page has embedded links back to 6.5.6 which is frankly infuriating. I also can't seem to access the APC FTP site to check and see if I can find it there. Would someone be able to provide me a link to 6.8.0, or baring that, is it possible to downgrade the whole unit (bootmon, AOS and APP) back to 6.5.6. Thank you all for your time.
Posted: 2022-05-03 07:21 PM
Hello,
I sent you a DM to download FW 6.8.0. I will also include FW 7.0.4 which is the latest.
Posted: 2022-05-20 01:35 AM
Same issue with trying to download the latest and greatest firmware for AP8659. They run on OS 6.8.2 (App 6.8.0) and because of some SNMP hicups I was looking for fresh firmware for the maintenance window... but.. am I doing something wrong? Why isn't it listed anywhere? Reasons I've missed? So weird. 7.0.4 is out as well... where did you find that? Cheers!
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.